Namespaces

The following namespaces are available for use, and included as part of the libraries that are provided with Microsoft's  implementation of the .NET Framework.

C#:

  •  System

  •  System.Collections.Generic

VB:

  •  System

  •  System.Collections.Generic

  •  Microsoft.VisualBasic

 

Namespaces defined

Reference: http://en.wikipedia.org/wiki/Base_Class_Library

License: The work is released under CC-BY-SA: http://creativecommons.org/licenses/by-sa/3.0/

System  

This namespace include the core needs for programming. It includes base types like String, DateTime, Boolean, and so forth, support for environments such as the console, math functions, and base classes for attributes, exceptions, and arrays.

 

System.Collections  

Defines many common containers or collections used in programming, such as lists, queues, stacks, hashtables, and dictionaries. It includes support for generics.

 

Microsoft.VisualBasic

Namespace contains types that support the Visual Basic Runtime in Visual Basic.

 

 


Related topics:

  

CSense 2023- Last updated: June 24,2025